AXIS#.VL.KIMODE

Description

This parameter sets whether the velocity mode is:

0 – Always on

1 – On ONLY if the position loop integrator is inactive.

AXIS#.PL.KITHRESH can be used to set a velocity command threshold to control at what part of a move the position loop integrator is active. When the position loop integrator becomes inactive, the velocity loop integrator will become active.

Usage

As a general rule, AXIS#.PL.KI should not be used at the same time as AXIS#.VL.KI , the two integrators will oppose each other and likely cause undesirable results, sometimes a runaway. Using AXIS#.PL.KITHRESH in conjunction with AXIS#.VL.KIMODE the user can specify operating conditions to switch between integrators based on machine operation.

Often times it makes sense to use the velocity integrator during a move, but as the motion comes to an end, to switch back to the position integrator for fine positioning.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1
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
AXIS1.VL.KIMODE

5011h

25h

Unsigned8

-

-

Read/Write

No

AXIS2.VL.KIMODE

5111h

25h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.KIMODE

6042

179A

Unsigned8

Read/Write

-

AXIS2.VL.KIMODE

71578

1179

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.KIMODE

6042

Unsigned8

Read/Write

-